Overview

Clips deliver constant pressure on board while protecting lens from mechanical overstress.
3 units are needed to operate a Fortimo FastFlex 2x8 module
2 units are needed to operate a Fortimo FastFlex 2x4 module

12NC: 929000948106
EOC: 871869643898500
If the product is not in stock in the Sample Webshop, it will be replenished from the Central Warehouse. The delivery time will be approximately five days longer, unless the product is not available in the Central Warehouse as well.
Product sample price: